Pin-out for Flexbus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin-out for Flexbus

1,613 Views
rowans-b
Contributor I

This is no doubt a beginner's question. I am considering using a K61 System on Module board for a project. I need the SoM to expose FlexBus, preferably 16 bits of address and 8 bits of data (non-multiplexed). Is the Flexbus presented on fixed pins of the K61 chip? If so, which ones? Or can I allocate Flexbus to any GPIO or other pins of the chip? If so, how, and what are the restrictions (if any)? Only if the SoM exposes the necessary address and data and read/write pins will it do the job I need...

Thanks for your help.

Rowan

0 Kudos
Reply
1 Reply

1,479 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Rowan,


Take a look at the table of Chapter 10.3.1 - Pin multiplexing and Pin Assignments of the reference manual of K61.

You will see that each pin has several muxing options. You can take out the FlexBus signals by different pins.

Regards,


Santiago