OTA update KW24D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTA update KW24D

1,423件の閲覧回数
edalmanzar
Contributor I

I'm trying to update my KW24D in the program NXP test tool 12 through OTA MAC and there is very little information about it. Someone could explain me the steps to made the ota update. 

I have changed the code, I have also tried another program with ota. But the KW24D remains unanswered to the ota update

#ota update‌

タグ(1)
0 件の賞賛
返信
1 返信

1,264件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please check the chapter 5. Over-the-air Programming of the IEEE 802.15.4 MAC Demo Applications User's Guide? 

This guide provides information about the 802.15.4 MAC Over-the-Air Programmer (MAC OTA Programmer) based on the Freescale 802.15.4 Media Access Controller (MAC) implementation.

The file it's located in the Connectivity Software of the KW24 under the path 

C:\<installation path>\MKW2xD_ConnSw_1.0.2\docs\wireless\IEEE 802.15.4

Regards, 

Estephania 

0 件の賞賛
返信