OPENSDAv2 for KEA128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OPENSDAv2 for KEA128

654 次查看
daweiyou
NXP Employee
NXP Employee

Hi:

I check the DAP source code, which doesn't include example for TRK-KEA128, pls help check where I could find the resource? thx.

标签 (1)
0 项奖励
回复
2 回复数

527 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Dawei,

     DO you mean the DAP source code is the oepnsdav2 MBED source code?

    That code is for the K20 chip, and used as the debugger, just like the FRDM on board debugger with MK20DX128VFM5, when you use the opensda v2.0, and change the firmware to JLINK, then the Jlink firmware will support the KEA128 chip.

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

527 次查看
daweiyou
NXP Employee
NXP Employee

got, thx Kerry.

Yes, I found source code for DAP, but it don't support KEA till now.

 The original debugger on TRK-KEA128 is from PE micro.

I want to implement simple flasher using DAP source code.

0 项奖励
回复