Need help with k70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help with k70

1,282 Views
sudeepaithal
Contributor I

Hello,can anyone please tell me if k70 MCU can deliver 3.3V signal from one pin(I/O pin) and 1.8v signal from another pin(I/O pin) simultaneously?If yes then which register should be access to make the necessary changes.

0 Kudos
Reply
1 Reply

1,165 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

For K70 has two DAC modules, customer can use one DAC module output 3.3V voltage and another DAC module output 1.8V voltage.

The K70 is single voltage powered, if customer using VDD 3.3V, then customer also could use one GPIO pin output 3.3V voltage and using a DAC module output 1.8V voltage.

Wish it helps.

best regards,

Ma Hui

0 Kudos
Reply