Minimum input voltage for edge capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum input voltage for edge capture

Jump to solution
2,461 Views
zorrotz
Contributor III

Hi,

In a KV4X, for a digital input, input voltage high is 0.7 x Vdd and input voltage low is 0.35 x Vdd.

Which are the minimum and maximum values for edge capture?

I have a sinusoidal signal of 200 mV peak in an input pin and I see that it is enough to detect falling/rising edges.

Thanks in advance

 

 

0 Kudos
Reply
1 Solution
2,370 Views
zorrotz
Contributor III

I have found why edges were being detected with such a low signal.

View solution in original post

0 Kudos
Reply
3 Replies
2,371 Views
zorrotz
Contributor III

I have found why edges were being detected with such a low signal.

0 Kudos
Reply
2,426 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zorrotz,

Please maintain the edges of the captured signal between 0.7 x Vdd and 0.35 x Vdd in order to ensure a proper edge detection of the signal.

 

0 Kudos
Reply
2,458 Views
zorrotz
Contributor III

I have forgotten to say that Vdd = 3.3 V

0 Kudos
Reply