MSCAN KEA-128 Rx all message id's

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSCAN KEA-128 Rx all message id's

1,387件の閲覧回数
vignesh_vb_7
Contributor IV

Hi,

I want to receive messages with all id's in MSCAN KEA-128 .

If I put Acceptance mask as 0xFFFFFFFF(extended id) or 0xFFF(standard id) then will i be able to receive all the messages?

0 件の賞賛
返信
1 返信

1,236件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

    If you want to receive all the Id's in MSCAN KEA128,  just configure all the MSCAN_CANIDMRn register to 0XFF, then you can receive all the ID, not matter extended ID or standard ID, and the according messages.

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信