MKW41Z - Debugger disconnects when VDD1P8 is increased

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW41Z - Debugger disconnects when VDD1P8 is increased

3,202 次查看
alexx_88
Contributor III

Hi,

I'm running a custom board with MKW41Z on it, powered from 3V3. In my hardware initialization routine (inspired from the FRDM-MKW41 examples), I'm increasing the output voltage of the built-in DC regulator from 1.8V to 2.6V. When that change takes effect, the board continues to run as expected, but the debugger (an LPCXpresso LPCLink 2) disconnects and the IDE (MCUXpresso 10.2.1)  throws an error and the debug session stops. The board continues to function as expected. Then I have to reset the board a couple of times until I'm able to erase the flash and reconnect with the debugger.

0 项奖励
回复
2 回复数

3,080 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Alexandru, I hope you're doing well!

 

Could you please try attaching the debug probe after the voltage change is performed to see if it can connect and continue the debug session?

 

This can be done while the probe is connected to your board, by choosing this option in MCUXpresso:

pastedImage_1.png

Please let me know if you still have issues.

 

Best regards,

Sebastian

0 项奖励
回复

3,080 次查看
alexx_88
Contributor III

Thanks, will try this and let you know :smileyhappy:

0 项奖励
回复