MKW01xxRM reference manual is missing the I2C chapter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKW01xxRM reference manual is missing the I2C chapter

1,343件の閲覧回数
theohill
Contributor I

I've got Rev. 2 - 3/2014 which as far as I can tell is the latest edition. There are numerous references to I2C in the manual (for example section 1.9.2), but no chapter describing the operation or memory map.

If it is documented elsewhere or if there is a similar I2C peripheral module that I can substitute the documentation for I'd appreciate being directed to that in addition to this manual being updated.

0 件の賞賛
返信
1 返信

1,261件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Theo,

You are right, there is a mistake in the MKW01xxRM. I confirm that there are two I2C modules inside the MKW01 MCU, these modules are the same as the included in the KL devices so the information in the MKL26 Reference Manual is valid for this peripheral.

Best regards,

Earl Ramírez.

0 件の賞賛
返信