MKV56F512VLL20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKV56F512VLL20

1,323件の閲覧回数
erskineb
Contributor I

Can anyone please post a link for initialization code for a MKV56F512VLL20? It is not listed in Processor Expert.  A project that can be imported into IAR would be great. I have found several locations on the Freescale Website that indicated its presents, but nothing there.

ラベル(1)
0 件の賞賛
返信
1 返信

1,151件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Erskine,

I've attached the startup and liker files of the KV31 instead of the KV56 , and you can port these files to the KV56 easily.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信