MKV31F256 2 Stop Bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKV31F256 2 Stop Bits

1,282件の閲覧回数
andreasruetten
Contributor III

Hello,

we have to use UART1 with  8N2.  ->  2 stop bits

Maybe i am blind, but i can't find any µC register for that.

Is it true, that the microcontroller doesn't have this feature?

If yes, is there a work arround?

 

Andreas

ラベル(1)
0 件の賞賛
返信
1 返信

1,273件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Refer to the RM, the uart only supports one stop bit. The data length can be 8 or 9. So you are right. We do not have 2 stop bit feature.

uart.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信