MKM34Z256VLL7 SWD interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM34Z256VLL7 SWD interface

2,189 Views
samdexter
Contributor II

Hi guys,

I've just finished a design of a board using MKM34Z256VLL7 and regretfully cannot program/debug it.

The SWD interface seems simple enough - all that it requires is Vtarget, GND, SWDIO and SWCLK.

However, I am not sure if it makes a use of RESET pin. Another thing is that the analog section on my

design is powered down.

So, I've got 2 questions:

1. Does SWD require RESET pin connected?

2. Does the micro have to be fully powered up, including the analog section in order to be programmed?

I presume it starts up with an internal oscillator (from the data sheet).

If anyone has any ideas please share...

Thank you very much.

Tags (1)
0 Kudos
Reply
1 Reply

2,080 Views
samdexter
Contributor II

Well, turns out I used wrong pin out for my j-link programming adapter...

Now, I guess, we know that the RESET pin is not required for SWD

and it does not matter if the analog section of the KM family powered

down.

Cheers.

0 Kudos
Reply