MKL15Z128VLH4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL15Z128VLH4

1,103 Views
punyatagayatri
Contributor II

Hi, I'm using MKL15Z128VLH4.Pls let me know if USB-ML-UNIVERSAL can be used as programmer/debugger?

Labels (2)
1 Reply

1,045 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Punyata Gayatri:

Yes, the Multilink Universal can be used with MKL15Z128VLH4. Just confirm that the tool is compatible with your chosen IDE. For example CodeWarrior, KDS, Keil and IAR support it.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------