MKL15Z128VLH4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL15Z128VLH4

1,102件の閲覧回数
punyatagayatri
Contributor II

Hi, I'm using MKL15Z128VLH4.Pls let me know if USB-ML-UNIVERSAL can be used as programmer/debugger?

ラベル(2)
1 返信

1,044件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Punyata Gayatri:

Yes, the Multilink Universal can be used with MKL15Z128VLH4. Just confirm that the tool is compatible with your chosen IDE. For example CodeWarrior, KDS, Keil and IAR support it.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------