MKE02z64VLC4 problem in interrupt execution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE02z64VLC4 problem in interrupt execution

3,466 Views
lavakushreddy
Contributor II

dear all,

i try to configure more than two interrupt's adc and  ftm for MKE02z64VLC4 controller

FTM interrupt works fine but my ADC interrupt doesn't get triggered , but if configure adc interrupt independently  it gets triggered,is it nvic priority issue.

please provide your valuable suggestions ASAP. 

Labels (1)
0 Kudos
Reply
5 Replies

3,144 Views
mjbcswitzerland
Specialist V

Hi

NVIC priorities handle when more than one interrupt occurs at the same time. Priority settings won't explain whey only one interrupt form 2 operates.

More likely you have disabled one interrupt source when enabling the other, or something similar. Read back the NVIC settings to ensure that both are really enabled.

Regards

Mark

0 Kudos
Reply

3,144 Views
lavakushreddy
Contributor II

Hi Mark,

thanks for your quick response,below is the code for configuring adc and ftm , i have compiled the code using IAR ,any issues in the below code.

#undef  VECTOR_035

#define VECTOR_035      FTM2_Isr        

#undef  VECTOR_031

#define VECTOR_031 ADC_Isr

extern void ADC_Isr(void);

extern void FTM2_Isr(void);

int main(void)

{

    ftm_init();

    adc_init();

     while(1)

{

]

}

void FTM2_Task(void)

{

  

      LED0_Toggle();   

}

void ADC_CallBack( void )

{

  LED0_Toggle();          /*!< toggle LED1 */

}

regards,

Lavakush

   

   void ftm_init(void)

   {

    SIM_RemapFTM2CH1Pin();

    SIM_RemapFTM2CH0Pin();

    /* FTM2 is set as edge aligned pwm mode, high true pulse */

    FTM_PWMInit(FTM2, FTM_PWMMODE_EDGEALLIGNED, FTM_PWM_HIGHTRUEPULSE);

    /* FTMEN enable */

    FTM_SetFTMEnhanced(FTM2);

    /* update MOD value */

    FTM_SetModValue(FTM2, 9999);

    /* set clock source, start counter */

    FTM_ClockSet(FTM2, FTM_CLOCK_SYSTEMCLOCK, FTM_CLOCK_PS_DIV1); 

    /* enable FTM2 interrupt in NVIC */

    NVIC_EnableIRQ(FTM2_IRQn);

    /* setup call back function for interrupt */

    FTM_SetCallback(FTM2, FTM2_Task);

    /* enable FTM2 overflow interrupt */

    FTM_EnableOverflowInt(FTM2);

  }

  void adc_init(void)

  {

    sADC_Config.u8ClockDiv = ADC_ADIV_DIVIDE_4;

    sADC_Config.u8ClockSource = CLOCK_SOURCE_BUS_CLOCK;

    sADC_Config.u8Mode = ADC_MODE_12BIT;

    sADC_Config.sSetting.bIntEn = 1;

    ADC_SetCallBack(ADC_CallBack);

    data=NVIC_GetPriority(ADC0_IRQn);

    ADC_Init( ADC, &sADC_Config);

   }

0 Kudos
Reply

3,144 Views
mjbcswitzerland
Specialist V

Hi

I see that the FTM interrupt is enabled using NVIC_EnableIRQ(FTM2_IRQn);

Shouldn't there be a similar call for the ADC?

Regards

Mark

0 Kudos
Reply

3,144 Views
lavakushreddy
Contributor II

hi mark,

i have enabled my interrupt by setting sADC_Config.sSetting.bIntEn = 1; below function takes care of calling NVIC_EnableIRQ() function

void ADC_Init(ADC_Type *pADC, ADC_ConfigTypePtr pADC_Config)

{

    if( pADC == ADC)

    {

        SIM->SCGC |= SIM_SCGC_ADC_MASK;

    }

    /* set clock cource for ADC */

    ADC_SelectClock(pADC,pADC_Config->u8ClockSource);

    /* set clock divide */

    ADC_SelectClockDivide(pADC,pADC_Config->u8ClockDiv);

    /* set ADC mode */

    ADC_SetMode(pADC,pADC_Config->u8Mode);

    /* set FIFO level */

    ADC_SetFifoLevel(pADC,pADC_Config->u8FiFoLevel);

    /* set pin control */

    pADC->APCTL1 = pADC_Config->u16PinControl;

    if( pADC_Config->sSetting.bCompareEn )

    {

        ADC_CompareEnable(pADC);

    }

   

    if( pADC_Config->sSetting.bCompareGreaterEn )

    {

        ADC_CompareGreaterFunction(pADC);

    }

       

    if( pADC_Config->sSetting.bContinuousEn )

    {

        ADC_ContinuousConversion(pADC);

    }

       

    if( pADC_Config->sSetting.bCompareAndEn )

    {

        ADC_CompareFifoAnd(pADC);

    }

   

    if( pADC_Config->sSetting.bFiFoScanModeEn )

    {

        ADC_FifoScanModeEnable(pADC);

    }

   

    if( pADC_Config->sSetting.bHardwareTriggerEn )

    {

        ADC_SetHardwareTrigger(pADC);

    }

    if( pADC_Config->sSetting.bIntEn )

    {

        ADC_IntEnable(pADC);

        NVIC_EnableIRQ( ADC0_IRQn );

    }

    if( pADC_Config->sSetting.bLongSampleEn )

    {

        ADC_SetLongSample(pADC);

    }

    if( pADC_Config->sSetting.bLowPowerEn )

    {

        ADC_SetLowPower(pADC);

    }

#if !defined(CPU_KE02)

    if( pADC_Config->sSetting.bHTRGMEn )

    {

        ADC_HardwareTriggerMultiple(pADC);

    }

    else

    {

  ADC_HardwareTriggerSingle(pADC);

    }

    if( pADC_Config->sSetting.bHTRGMASKEn )

    {

        ADC_HardwareTriggerMaskEnable(pADC);

    }

    else

    {

  ADC_HardwareTriggerMaskDisable(pADC);

    }

    if( pADC_Config->sSetting.bHTRGMASKSEL )

    {

        ADC_HardwareTriggerMaskAuto(pADC);

    }

    else

    {

  ADC_HardwareTriggerMaskNonAuto(pADC);

    }

#endif

}

0 Kudos
Reply

3,144 Views
pramodtm-b46240
Contributor III

Hi lavakush,

     Not setting the priority for interrupts can also cause such issues. The other reason might be that NMI pin is not disabled. By default NMI pin is enabled. Processor expert has a setting to disable NMI setting. But if you are developing a baremetal code, this needs to be disabled during initialization.

0 Kudos
Reply