MK64FN1M0VLL12 reset problem after power failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64FN1M0VLL12 reset problem after power failure

ソリューションへジャンプ
2,313件の閲覧回数
f_schwamborn
Contributor I

Hello,

i use a MK64FN1M0VLL12 processor on 2 applications, a FRDM-K64f board and a custom application. I noticed that the processor would not boot after longer power failures (> than 20 seconds) and only a manual reset makes the processor boot again. Shorter periods do not lead to this behaviour.

The ethernet phy does not seem to fail because it provides a stable 50MHz clock output.

Does anyone have an idea, what may cause this problem ?

Regards

Fabian

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,073件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi Fabian,

This issue was already discussed, check this thread:

FRDM-K64F booting issue when powered from USB port


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,074件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi Fabian,

This issue was already discussed, check this thread:

FRDM-K64F booting issue when powered from USB port


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,073件の閲覧回数
f_schwamborn
Contributor I

Hello,

thank you for your help. I had the same issue with a capacitor on the NMI pin.

Best regards,

Fabian

0 件の賞賛
返信