MK60FN1xxx12 - SD Card Bare Metal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60FN1xxx12 - SD Card Bare Metal

1,173 Views
jgreene
Contributor I

Hello,

I've been looking for a bare metal driver example for SD card functionality on the MK60FN1xxx12 processor. I've found several examples for similar processor but have had a difficult time finding one for this particular processor that didn't need a significant amount of changes to be made.

 

Thank you in advance,

Jon

0 Kudos
Reply
1 Reply

1,166 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jgreene,

  We don't have the directly K60 120M sdcard sample code, but you can refer to the K60D100 sdk code, that code contains the sdcard driver and sample code.

 You can donwload SDK_2.2.0_TWR-K60D100M from this link:

https://mcuxpresso.nxp.com/en/select

Then the sdcard code folder:

SDK_2.2.0_TWR-K60D100M\boards\twrk60d100m\driver_examples\sdcard

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 Kudos
Reply