MK60DN512VMD10 / MK60DN512ZVMD10 Comparator Input Differences

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512VMD10 / MK60DN512ZVMD10 Comparator Input Differences

2,661 Views
PhilV
Contributor III

I am trying to configure a project that will run on both the MK60DN512 and the earlier MK60DN512Z parts, but I am having an issue with the comparator inputs.

The reference manual for the Z part shows:

Z-comparator_RM.png

and the equivalent table for the non Z version shows:

PhilV_1-1643050435842.png

However, I have looked through the AN4445 application note that details what was changed between 1.x silicon and 2.x, and it doesn't seem to be mentioned.
The only other mention of the CMP#_IN2 input is right at the end of the non-Z version document, in the appendix where it details document changes for version 2 of the document:

 

PhilV_1-1643050646450.png

but it doesn't indicate why those changes were made to the document.

Does the Z device really not have those internal connections, or was it a problem with the document which was later rectified?

Thanks!

 

Labels (1)
0 Kudos
Reply
3 Replies

2,649 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @PhilV :

Thanks for the observations, but in new documents, (both MK60DN512 with and without z) have cmp input connection the same in the table. So, theoretically the configuration and the portability should be the same

Here is where you can download the newest document

https://www.nxp.com/webapp/Download?colCode=K60P144M100SF2V2RM (page 128)

https://www.nxp.com/webapp/Download?colCode=K60P120M100SF2RM  (page 121)

I hope this help you

2,636 Views
PhilV
Contributor III

Hi @CarlosGarabito ,

Thanks for the links, however the K60P120M100SF2RM document says it only supports the MK60DN512ZCAB10 device, whereas I am using the MK60DN512ZVMD10 (I have now updated the ticket title to reflect this) - the latest manual for which (from THIS PAGE) seems to be "Rev. 6, Nov 2011".

 

0 Kudos
Reply

2,622 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

OK, the file you can use for this micro is https://www.nxp.com/webapp/Download?colCode=K60P121M100SF2V2RM .

 

Just for information, you can know the difference between the nomenclatures of the micros that are similar using the format table (page 5 on the document Kinetis K60: 100MHz Cortex-M4 256/512KB Flash (121 pin) (nxp.com)).

 

tabla1.pngtabla2.png

0 Kudos
Reply