MK30D10 (100MHZ) FlexCAN issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK30D10 (100MHZ) FlexCAN issue

1,826件の閲覧回数
i_smailtatlınar
Contributor I

I was trying to use RX Fifo for K30D10 FlexCan module. Reference manual says there is 64 MB could be use and up to 128 Fifo Filter could be use. But, I realized that I cannot use more then 16 MB. I could not reach CS16 register in example. At CTRL2[RFFN] register there is a table. RFFN could be 3 maximum. But there is nothing about this limitation. Do I have to something to use full functional CAN?

タグ(3)
1 返信

1,733件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Tatlinar,

Pls refer to the section in RM of K30, I copy it here:

"

3.9.1.3 Number of message buffers
Each FlexCAN module contains 16 message buffers. Each message buffer is 16 bytes.

"

It means that the RAM size is 16* 16=256 bytes.

Hope it can help you

BR

Xiangjun Rong