MK22FN128VDC10 package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK22FN128VDC10 package

ソリューションへジャンプ
4,185件の閲覧回数
sergeysokolov
Contributor I

What is the correct name of MK22FN128VDC10 package, MAPBGA 121 8*8*0.5 P0.65 or 121 XFBGA? is it the same?

0 件の賞賛
返信
1 解決策
4,036件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sergey,

Of course, you can refer to the application note.

And I think it's a very helpful file.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,037件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sergey,

Of course, you can refer to the application note.

And I think it's a very helpful file.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,036件の閲覧回数
sergeysokolov
Contributor I

Thank you

the last question - can I consider AN3846 as PCB Design Guidelines for this package?

0 件の賞賛
返信
4,036件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sergey,

The kind package of the MK22FN128VDC10 IS XFBGA, 121 8*8*0.5, and I've also attached the package description and mechanical drawing.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,036件の閲覧回数
sergeysokolov
Contributor I

Hi Ping,

I saw this document, but package there called MAPBGA

0 件の賞賛
返信
4,036件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sergey,

After verified the kind of parameters that the file illustrates, I think it's a doc issue, the title should be the XFBGA instead of the MAPBGA.

And I'll report the issue to the doc team later.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信