MK22 RTC powering through VDD of controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK22 RTC powering through VDD of controller

2,585件の閲覧回数
vaibhavi_padwal
Contributor II

Hi,

I am using MK22FX5120AVLQ12 controller on my custom board. I am using RTC module with crystal of 32.768kHz and an external battery on VBAT pins. As per reference manual, the module is power through only VBAT pin supply in both Chip power down and Chip power up mode. (please see the attached screenshot) 

1. I would like to know if there's any provision to configure the RTC module to take power from VDD supply when the controller is powered ON.

2. Sometimes the RTC time gets reset to the default time. This event happens randomly and I have observed it on multiple boards. I have also confirmed that this is not because of battery draining. I measured the external battery voltage and found it to be near 3.1V which is the actual battery voltage. What could be the potential causes behind this?

Thanks & Regards,

Vaibhavi Padwal

ラベル(1)
0 件の賞賛
返信
1 返信

2,543件の閲覧回数
vaibhavi_padwal
Contributor II

Hi,

Kindly help in resolving above mentioned queries.

Thanks & Regards,

Vaibhavi 

0 件の賞賛
返信