MK21 DMA SPI2 problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK21 DMA SPI2 problems

Jump to solution
5,826 Views
DaniMartin
Contributor II

Hi,

I'm trying to transmit data via SPI2 peripheral, using DMA in my MK21FX512AVMD12. I'm looking at the drivers examples (twrk21f120m_dspi_edma_b2b_transfer_master, twrk21f120m_dspi_half_duplex_edma_master)....and I see diferences when I use SPI2 instead SPI0. In those examples for the SPI0 peripheral the callback is called adequately, but when I change to SPI2, it is not called. These are the changes that I apply:

DaniMartin_0-1660221226656.png

 

In the edma_spi driver it is clear that both peripherals are different, because SPI0 has separate DMA request and SPI2 don't.

Do I have to change anything else in order to use SPI2?

Labels (1)
0 Kudos
Reply
1 Solution
5,725 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I could not get the twr-k21 but I make some tests with the frdm-k22 this is the code I modified and tested.

 

 

Spoiler
/*
 * Copyright (c) 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "fsl_dspi.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_dspi_edma.h"
#include "fsl_edma.h"
#include "fsl_dmamux.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define EXAMPLE_DSPI_MASTER_BASEADDR              SPI1
#define EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR      DMAMUX
#define EXAMPLE_DSPI_MASTER_DMA_BASEADDR          DMA0
#define EXAMPLE_DSPI_MASTER_DMA_TX_RX_REQUEST_SOURCE kDmaRequestMux0SPI1
//#define EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE kDmaRequestMux0SPI0Tx
#define DSPI_MASTER_CLK_SRC                       DSPI1_CLK_SRC
#define DSPI_MASTER_CLK_FREQ                      CLOCK_GetFreq(DSPI1_CLK_SRC)
#define EXAMPLE_DSPI_MASTER_PCS_FOR_INIT          kDSPI_Pcs0
#define EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER      kDSPI_MasterPcs0
#define EXAMPLE_DSPI_DEALY_COUNT                  0xfffffU
#define TRANSFER_SIZE     64U     /* Transfer dataSize */
#define TRANSFER_BAUDRATE 500000U /* Transfer baudrate - 500k */

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
/* DSPI user callback */
void DSPI_MasterUserCallback(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData);

/*******************************************************************************
 * Variables
 ******************************************************************************/
uint8_t masterRxData[TRANSFER_SIZE] = {0};
uint8_t masterTxData[TRANSFER_SIZE] = {0};

dspi_master_edma_handle_t g_dspi_edma_m_handle;
edma_handle_t dspiEdmaMasterRxRegToRxDataHandle;
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
edma_handle_t dspiEdmaMasterTxDataToIntermediaryHandle;
#endif
edma_handle_t dspiEdmaMasterIntermediaryToTxRegHandle;

volatile bool isTransferCompleted  = false;
volatile uint32_t g_systickCounter = 20U;
/*******************************************************************************
 * Code
 ******************************************************************************/
void SysTick_Handler(void)
{
    if (g_systickCounter != 0U)
    {
        g_systickCounter--;
    }
}

void DSPI_MasterUserCallback(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData)
{
    if (status == kStatus_Success)
    {
        PRINTF("This is DSPI master edma transfer completed callback. \r\n\r\n");
    }

    isTransferCompleted = true;
}

/*!
 * @brief Main function
 */
int main(void)
{
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitDebugConsole();

    PRINTF("DSPI board to board edma example.\r\n");
    PRINTF("This example use one board as master and another as slave.\r\n");
    PRINTF("Master and slave uses EDMA way. Slave should start first. \r\n");
    PRINTF("Please make sure you make the correct line connection. Basically, the connection is: \r\n");
    PRINTF("DSPI_master -- DSPI_slave   \r\n");
    PRINTF("   CLK      --    CLK  \r\n");
    PRINTF("   PCS      --    PCS \r\n");
    PRINTF("   SOUT     --    SIN  \r\n");
    PRINTF("   SIN      --    SOUT \r\n");
    PRINTF("   GND      --    GND \r\n");

    /* DMA Mux setting and EDMA init */
    uint32_t masterRxChannel, masterTxChannel;
    edma_config_t userConfig;

    masterRxChannel = 0U;
    masterTxChannel = 1U;
/* If DSPI instances support Gasket feature, only two channels are needed. */
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    uint32_t masterIntermediaryChannel;
    masterIntermediaryChannel = 2U;
#endif
    /* DMA MUX init */
    DMAMUX_Init(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR);

    DMAMUX_SetSource(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterRxChannel, (uint8_t)EXAMPLE_DSPI_MASTER_DMA_TX_RX_REQUEST_SOURCE);
    DMAMUX_EnableChannel(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterRxChannel);

#if (defined EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE)
    DMAMUX_SetSource(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterTxChannel, (uint8_t)EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE);
    DMAMUX_EnableChannel(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterTxChannel);
#endif

    /* EDMA init */
    /*
     * userConfig.enableRoundRobinArbitration = false;
     * userConfig.enableHaltOnError = true;
     * userConfig.enableContinuousLinkMode = false;
     * userConfig.enableDebugMode = false;
     */
    EDMA_GetDefaultConfig(&userConfig);

    EDMA_Init(EXAMPLE_DSPI_MASTER_DMA_BASEADDR, &userConfig);

    uint32_t srcClock_Hz;
    uint32_t errorCount;
    uint32_t loopCount = 1U;
    uint32_t i;
    dspi_master_config_t masterConfig;
    dspi_transfer_t masterXfer;

    /* Master config */
    masterConfig.whichCtar                                = kDSPI_Ctar0;
    masterConfig.ctarConfig.baudRate                      = TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.bitsPerFrame                  = 8;
    masterConfig.ctarConfig.cpol                          = kDSPI_ClockPolarityActiveHigh;
    masterConfig.ctarConfig.cpha                          = kDSPI_ClockPhaseFirstEdge;
    masterConfig.ctarConfig.direction                     = kDSPI_MsbFirst;
    masterConfig.ctarConfig.pcsToSckDelayInNanoSec        = 1000000000U / TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.lastSckToPcsDelayInNanoSec    = 1000000000U / TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.betweenTransferDelayInNanoSec = 1000000000U / TRANSFER_BAUDRATE;

    masterConfig.whichPcs           = EXAMPLE_DSPI_MASTER_PCS_FOR_INIT;
    masterConfig.pcsActiveHighOrLow = kDSPI_PcsActiveLow;

    masterConfig.enableContinuousSCK        = false;
    masterConfig.enableRxFifoOverWrite      = false;
    masterConfig.enableModifiedTimingFormat = false;
    masterConfig.samplePoint                = kDSPI_SckToSin0Clock;

    srcClock_Hz = DSPI_MASTER_CLK_FREQ;
    DSPI_MasterInit(EXAMPLE_DSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

    /* Set up dspi master */
    memset(&(dspiEdmaMasterRxRegToRxDataHandle), 0, sizeof(dspiEdmaMasterRxRegToRxDataHandle));
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    memset(&(dspiEdmaMasterTxDataToIntermediaryHandle), 0, sizeof(dspiEdmaMasterTxDataToIntermediaryHandle));
#endif
    memset(&(dspiEdmaMasterIntermediaryToTxRegHandle), 0, sizeof(dspiEdmaMasterIntermediaryToTxRegHandle));

    EDMA_CreateHandle(&(dspiEdmaMasterRxRegToRxDataHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterRxChannel);
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    EDMA_CreateHandle(&(dspiEdmaMasterTxDataToIntermediaryHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterIntermediaryChannel);
#endif
    EDMA_CreateHandle(&(dspiEdmaMasterIntermediaryToTxRegHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterTxChannel);
#if (defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET)
    DSPI_MasterTransferCreateHandleEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, DSPI_MasterUserCallback,
                                        NULL, &dspiEdmaMasterRxRegToRxDataHandle, NULL,
                                        &dspiEdmaMasterIntermediaryToTxRegHandle);
#else
    DSPI_MasterTransferCreateHandleEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, DSPI_MasterUserCallback,
                                        NULL, &dspiEdmaMasterRxRegToRxDataHandle,
                                        &dspiEdmaMasterTxDataToIntermediaryHandle,
                                        &dspiEdmaMasterIntermediaryToTxRegHandle);
#endif

    while (1)
    {
        /* Set up the transfer data */
        for (i = 0U; i < TRANSFER_SIZE; i++)
        {
            masterTxData[i] = (i + loopCount) % 256U;
            masterRxData[i] = 0U;
        }

        /* Print out transmit buffer */
        PRINTF("\r\n Master transmit:\r\n");
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            /* Print 16 numbers in a line */
            if ((i & 0x0FU) == 0U)
            {
                PRINTF("\r\n");
            }
            PRINTF(" %02X", masterTxData[i]);
        }
        PRINTF("\r\n");

        /* Start master transfer, send data to slave */
        isTransferCompleted    = false;
        masterXfer.txData      = masterTxData;
        masterXfer.rxData      = NULL;
        masterXfer.dataSize    = TRANSFER_SIZE;
        masterXfer.configFlags = kDSPI_MasterCtar0 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterPcsContinuous;
        if (kStatus_Success !=
            DSPI_MasterTransferEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, &masterXfer))
        {
            PRINTF("There is error when start DSPI_MasterTransferEDMA \r\n ");
        }

        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        /* Delay to wait slave is ready */
        if (SysTick_Config(SystemCoreClock / 1000U))
        {
            while (1)
            {
            }
        }
        /* Delay 20 ms */
        g_systickCounter = 20U;
        while (g_systickCounter != 0U)
        {
        }

        /* Start master transfer, receive data from slave */
        isTransferCompleted    = false;
        masterXfer.txData      = NULL;
        masterXfer.rxData      = masterRxData;
        masterXfer.dataSize    = TRANSFER_SIZE;
        masterXfer.configFlags = kDSPI_MasterCtar0 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterPcsContinuous;
        if (kStatus_Success !=
            DSPI_MasterTransferEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, &masterXfer))
        {
            PRINTF("There is error when start DSPI_MasterTransferEDMA \r\n ");
        }

        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        errorCount = 0;
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            if (masterTxData[i] != masterRxData[i])
            {
                errorCount++;
            }
        }
        if (errorCount == 0)
        {
            PRINTF(" \r\nDSPI transfer all data matched! \r\n");
            /* Print out receive buffer */
            PRINTF("\r\n Master received:\r\n");
            for (i = 0; i < TRANSFER_SIZE; i++)
            {
                /* Print 16 numbers in a line */
                if ((i & 0x0FU) == 0U)
                {
                    PRINTF("\r\n");
                }
                PRINTF(" %02X", masterRxData[i]);
            }
            PRINTF("\r\n");
        }
        else
        {
            PRINTF(" \r\nError occurred in DSPI transfer ! \r\n");
        }

        /* Wait for press any key */
        PRINTF("\r\n Press any key to run again\r\n");
        GETCHAR();
        /* Increase loop count to change transmit buffer */
        loopCount++;
    }
}

I think this could help you to port in the k21. 

 

Best regards,
Pavel

View solution in original post

7 Replies
5,790 Views
DaniMartin
Contributor II

Hi @Pavel_Hernandez , thanks for the answer. I already try to use only one macro (disabling the RX part), but it is not working. The callback is not being called:

DaniMartin_0-1660630152943.png

(...)

DaniMartin_1-1660630174575.png

 

0 Kudos
Reply
5,781 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I suggest reviewing the code because in the original code there are using 2 sources of the DMAMUX but with the SPI2 you need to modify your code to use only one source.

Pavel_Hernandez_0-1660772664245.png

This configuration handler is for an inexistent source.

Pavel_Hernandez_1-1660772829288.png

Best regards,
Pavel

0 Kudos
Reply
5,777 Views
DaniMartin
Contributor II

What do you mean to reviewing the code? Please, could you send the  twrk21f120m_dspi_edma_b2b_transfer_master example working for SPI2?

 

thanks

0 Kudos
Reply
5,766 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Let me get 2 twr-k21 for making a test.

Best regards,
Pavel

5,726 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I could not get the twr-k21 but I make some tests with the frdm-k22 this is the code I modified and tested.

 

 

Spoiler
/*
 * Copyright (c) 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "fsl_dspi.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_dspi_edma.h"
#include "fsl_edma.h"
#include "fsl_dmamux.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define EXAMPLE_DSPI_MASTER_BASEADDR              SPI1
#define EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR      DMAMUX
#define EXAMPLE_DSPI_MASTER_DMA_BASEADDR          DMA0
#define EXAMPLE_DSPI_MASTER_DMA_TX_RX_REQUEST_SOURCE kDmaRequestMux0SPI1
//#define EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE kDmaRequestMux0SPI0Tx
#define DSPI_MASTER_CLK_SRC                       DSPI1_CLK_SRC
#define DSPI_MASTER_CLK_FREQ                      CLOCK_GetFreq(DSPI1_CLK_SRC)
#define EXAMPLE_DSPI_MASTER_PCS_FOR_INIT          kDSPI_Pcs0
#define EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER      kDSPI_MasterPcs0
#define EXAMPLE_DSPI_DEALY_COUNT                  0xfffffU
#define TRANSFER_SIZE     64U     /* Transfer dataSize */
#define TRANSFER_BAUDRATE 500000U /* Transfer baudrate - 500k */

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
/* DSPI user callback */
void DSPI_MasterUserCallback(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData);

/*******************************************************************************
 * Variables
 ******************************************************************************/
uint8_t masterRxData[TRANSFER_SIZE] = {0};
uint8_t masterTxData[TRANSFER_SIZE] = {0};

dspi_master_edma_handle_t g_dspi_edma_m_handle;
edma_handle_t dspiEdmaMasterRxRegToRxDataHandle;
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
edma_handle_t dspiEdmaMasterTxDataToIntermediaryHandle;
#endif
edma_handle_t dspiEdmaMasterIntermediaryToTxRegHandle;

volatile bool isTransferCompleted  = false;
volatile uint32_t g_systickCounter = 20U;
/*******************************************************************************
 * Code
 ******************************************************************************/
void SysTick_Handler(void)
{
    if (g_systickCounter != 0U)
    {
        g_systickCounter--;
    }
}

void DSPI_MasterUserCallback(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData)
{
    if (status == kStatus_Success)
    {
        PRINTF("This is DSPI master edma transfer completed callback. \r\n\r\n");
    }

    isTransferCompleted = true;
}

/*!
 * @brief Main function
 */
int main(void)
{
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitDebugConsole();

    PRINTF("DSPI board to board edma example.\r\n");
    PRINTF("This example use one board as master and another as slave.\r\n");
    PRINTF("Master and slave uses EDMA way. Slave should start first. \r\n");
    PRINTF("Please make sure you make the correct line connection. Basically, the connection is: \r\n");
    PRINTF("DSPI_master -- DSPI_slave   \r\n");
    PRINTF("   CLK      --    CLK  \r\n");
    PRINTF("   PCS      --    PCS \r\n");
    PRINTF("   SOUT     --    SIN  \r\n");
    PRINTF("   SIN      --    SOUT \r\n");
    PRINTF("   GND      --    GND \r\n");

    /* DMA Mux setting and EDMA init */
    uint32_t masterRxChannel, masterTxChannel;
    edma_config_t userConfig;

    masterRxChannel = 0U;
    masterTxChannel = 1U;
/* If DSPI instances support Gasket feature, only two channels are needed. */
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    uint32_t masterIntermediaryChannel;
    masterIntermediaryChannel = 2U;
#endif
    /* DMA MUX init */
    DMAMUX_Init(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR);

    DMAMUX_SetSource(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterRxChannel, (uint8_t)EXAMPLE_DSPI_MASTER_DMA_TX_RX_REQUEST_SOURCE);
    DMAMUX_EnableChannel(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterRxChannel);

#if (defined EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE)
    DMAMUX_SetSource(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterTxChannel, (uint8_t)EXAMPLE_DSPI_MASTER_DMA_TX_REQUEST_SOURCE);
    DMAMUX_EnableChannel(EXAMPLE_DSPI_MASTER_DMA_MUX_BASEADDR, masterTxChannel);
#endif

    /* EDMA init */
    /*
     * userConfig.enableRoundRobinArbitration = false;
     * userConfig.enableHaltOnError = true;
     * userConfig.enableContinuousLinkMode = false;
     * userConfig.enableDebugMode = false;
     */
    EDMA_GetDefaultConfig(&userConfig);

    EDMA_Init(EXAMPLE_DSPI_MASTER_DMA_BASEADDR, &userConfig);

    uint32_t srcClock_Hz;
    uint32_t errorCount;
    uint32_t loopCount = 1U;
    uint32_t i;
    dspi_master_config_t masterConfig;
    dspi_transfer_t masterXfer;

    /* Master config */
    masterConfig.whichCtar                                = kDSPI_Ctar0;
    masterConfig.ctarConfig.baudRate                      = TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.bitsPerFrame                  = 8;
    masterConfig.ctarConfig.cpol                          = kDSPI_ClockPolarityActiveHigh;
    masterConfig.ctarConfig.cpha                          = kDSPI_ClockPhaseFirstEdge;
    masterConfig.ctarConfig.direction                     = kDSPI_MsbFirst;
    masterConfig.ctarConfig.pcsToSckDelayInNanoSec        = 1000000000U / TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.lastSckToPcsDelayInNanoSec    = 1000000000U / TRANSFER_BAUDRATE;
    masterConfig.ctarConfig.betweenTransferDelayInNanoSec = 1000000000U / TRANSFER_BAUDRATE;

    masterConfig.whichPcs           = EXAMPLE_DSPI_MASTER_PCS_FOR_INIT;
    masterConfig.pcsActiveHighOrLow = kDSPI_PcsActiveLow;

    masterConfig.enableContinuousSCK        = false;
    masterConfig.enableRxFifoOverWrite      = false;
    masterConfig.enableModifiedTimingFormat = false;
    masterConfig.samplePoint                = kDSPI_SckToSin0Clock;

    srcClock_Hz = DSPI_MASTER_CLK_FREQ;
    DSPI_MasterInit(EXAMPLE_DSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

    /* Set up dspi master */
    memset(&(dspiEdmaMasterRxRegToRxDataHandle), 0, sizeof(dspiEdmaMasterRxRegToRxDataHandle));
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    memset(&(dspiEdmaMasterTxDataToIntermediaryHandle), 0, sizeof(dspiEdmaMasterTxDataToIntermediaryHandle));
#endif
    memset(&(dspiEdmaMasterIntermediaryToTxRegHandle), 0, sizeof(dspiEdmaMasterIntermediaryToTxRegHandle));

    EDMA_CreateHandle(&(dspiEdmaMasterRxRegToRxDataHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterRxChannel);
#if (!(defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET))
    EDMA_CreateHandle(&(dspiEdmaMasterTxDataToIntermediaryHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterIntermediaryChannel);
#endif
    EDMA_CreateHandle(&(dspiEdmaMasterIntermediaryToTxRegHandle), EXAMPLE_DSPI_MASTER_DMA_BASEADDR, masterTxChannel);
#if (defined(FSL_FEATURE_DSPI_HAS_GASKET) && FSL_FEATURE_DSPI_HAS_GASKET)
    DSPI_MasterTransferCreateHandleEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, DSPI_MasterUserCallback,
                                        NULL, &dspiEdmaMasterRxRegToRxDataHandle, NULL,
                                        &dspiEdmaMasterIntermediaryToTxRegHandle);
#else
    DSPI_MasterTransferCreateHandleEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, DSPI_MasterUserCallback,
                                        NULL, &dspiEdmaMasterRxRegToRxDataHandle,
                                        &dspiEdmaMasterTxDataToIntermediaryHandle,
                                        &dspiEdmaMasterIntermediaryToTxRegHandle);
#endif

    while (1)
    {
        /* Set up the transfer data */
        for (i = 0U; i < TRANSFER_SIZE; i++)
        {
            masterTxData[i] = (i + loopCount) % 256U;
            masterRxData[i] = 0U;
        }

        /* Print out transmit buffer */
        PRINTF("\r\n Master transmit:\r\n");
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            /* Print 16 numbers in a line */
            if ((i & 0x0FU) == 0U)
            {
                PRINTF("\r\n");
            }
            PRINTF(" %02X", masterTxData[i]);
        }
        PRINTF("\r\n");

        /* Start master transfer, send data to slave */
        isTransferCompleted    = false;
        masterXfer.txData      = masterTxData;
        masterXfer.rxData      = NULL;
        masterXfer.dataSize    = TRANSFER_SIZE;
        masterXfer.configFlags = kDSPI_MasterCtar0 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterPcsContinuous;
        if (kStatus_Success !=
            DSPI_MasterTransferEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, &masterXfer))
        {
            PRINTF("There is error when start DSPI_MasterTransferEDMA \r\n ");
        }

        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        /* Delay to wait slave is ready */
        if (SysTick_Config(SystemCoreClock / 1000U))
        {
            while (1)
            {
            }
        }
        /* Delay 20 ms */
        g_systickCounter = 20U;
        while (g_systickCounter != 0U)
        {
        }

        /* Start master transfer, receive data from slave */
        isTransferCompleted    = false;
        masterXfer.txData      = NULL;
        masterXfer.rxData      = masterRxData;
        masterXfer.dataSize    = TRANSFER_SIZE;
        masterXfer.configFlags = kDSPI_MasterCtar0 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterPcsContinuous;
        if (kStatus_Success !=
            DSPI_MasterTransferEDMA(EXAMPLE_DSPI_MASTER_BASEADDR, &g_dspi_edma_m_handle, &masterXfer))
        {
            PRINTF("There is error when start DSPI_MasterTransferEDMA \r\n ");
        }

        /* Wait until transfer completed */
        while (!isTransferCompleted)
        {
        }

        errorCount = 0;
        for (i = 0; i < TRANSFER_SIZE; i++)
        {
            if (masterTxData[i] != masterRxData[i])
            {
                errorCount++;
            }
        }
        if (errorCount == 0)
        {
            PRINTF(" \r\nDSPI transfer all data matched! \r\n");
            /* Print out receive buffer */
            PRINTF("\r\n Master received:\r\n");
            for (i = 0; i < TRANSFER_SIZE; i++)
            {
                /* Print 16 numbers in a line */
                if ((i & 0x0FU) == 0U)
                {
                    PRINTF("\r\n");
                }
                PRINTF(" %02X", masterRxData[i]);
            }
            PRINTF("\r\n");
        }
        else
        {
            PRINTF(" \r\nError occurred in DSPI transfer ! \r\n");
        }

        /* Wait for press any key */
        PRINTF("\r\n Press any key to run again\r\n");
        GETCHAR();
        /* Increase loop count to change transmit buffer */
        loopCount++;
    }
}

I think this could help you to port in the k21. 

 

Best regards,
Pavel

5,717 Views
DaniMartin
Contributor II

thanks!! It works in MK21 for both SPI1 and SP2.

 

5,814 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I review the example and I confirm something in the Reference Manual in the section [Table 3-25. DMA request sources - MUX 0] you can see the sources of the example in yellow.

Pavel_Hernandez_0-1660341883877.png

Pavel_Hernandez_1-1660342001458.png

But the SPI2 only have 1 source for transmit or Receive, and you define tow macros but only need one.

 

#define EXAMPLE_DSPI_MASTER_DMA_RX_TX_REQUEST_SOURCE kDmaRequestMux0SPI2

 

Try it and if you have more questions please let me know.

Best regards,
Pavel

0 Kudos
Reply