MK20DN512ZVLQ10 USB FAILURES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DN512ZVLQ10 USB FAILURES

1,319件の閲覧回数
kevinmc
Junior Contributor II

We manufacture 3 products with this component.

We have numerous instances (100+) instance of the product having been assembled and programmed with a Cyclone production programmer, then fails when connected to USB.

The equipment is not seen by the host computer and the micro-controller gets extremely hot.

This issue only occurs if USB is connected. Other operations are unaffected.

95% of product appears OK and has no issue on the USB in either removable disk or COM port mode.

Does anybody have any similar problems with this device failure mode? Is it a common issue with the USB?

Is this a common mode of device failure?

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
1 返信

1,238件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kevin

have you check that there is not any manufacturer problem like a solder short or missing part?

Maybe you have a solder short on the USB area.

regards

Vicente Gomez

0 件の賞賛
返信