MK20 not booting after power cycle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20 not booting after power cycle

1,641 Views
felixgottwald
Contributor I

Hi.

We use a MK20DX256 on our own boards. Thereby we have a strange behavior after booting. The device does not go to the main routine after start up. If we toggle the RESET pin manually to low, the user program starts running and everything works fine. The RESET pin is connected with a 10k resistor to VCC and with 100nF to GND. We have no idea what is the problem, maybe the controller goes in bootloader mode after a regular power cycle or something like that.

Do you have an idea in which direction we have to look for a solution for this problem?

Thank you for your help.

Regards Felix

Tags (2)
0 Kudos
Reply
1 Reply

1,532 Views
felixgottwald
Contributor I

I´ve solved my issue by disableing "EzPort operation at boot" in the Cpu Properties (Advanced Mode) in ProcessorExpert.

Regards

0 Kudos
Reply