MK10DX64VLH7 KSDK1.3.0 libraries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK10DX64VLH7 KSDK1.3.0 libraries

1,213件の閲覧回数
rogerpease
Contributor III

I am looking to use an MK10DX64VLH7 with KSDK 1.3.0 to do some flash programming. 

I looked through the devices in the list of supported parts for that library and couldn't find this device. Can someone identify a similar one that I could use as a starting point? I gather name-similarity is not a good indicator as MKV10DX64VLH7 is a different processor and MK10DX64xxx10 has (I believe) different peripherals. 

09/25/2020 02:13 PM <DIR> MK02F12810
09/25/2020 02:13 PM <DIR> MK10D10
09/25/2020 02:13 PM <DIR> MK11DA5
09/25/2020 02:13 PM <DIR> MK20D10
09/25/2020 02:13 PM <DIR> MK21DA5
09/25/2020 02:13 PM <DIR> MK21FA12
09/25/2020 02:13 PM <DIR> MK22F12810
09/25/2020 02:13 PM <DIR> MK22F25612
09/25/2020 02:13 PM <DIR> MK22F51212
09/24/2020 03:15 PM <DIR> MK22FA12
09/25/2020 02:13 PM <DIR> MK24F12
09/25/2020 02:13 PM <DIR> MK24F25612
09/25/2020 02:13 PM <DIR> MK26F18
09/25/2020 02:13 PM <DIR> MK30D10
09/25/2020 02:13 PM <DIR> MK40D10
09/25/2020 02:13 PM <DIR> MK50D10
09/25/2020 02:13 PM <DIR> MK51D10
09/25/2020 02:13 PM <DIR> MK52D10
09/25/2020 02:13 PM <DIR> MK53D10
09/25/2020 02:13 PM <DIR> MK60D10
09/25/2020 02:13 PM <DIR> MK63F12
09/25/2020 02:13 PM <DIR> MK64F12
09/25/2020 02:13 PM <DIR> MK65F18
09/25/2020 02:13 PM <DIR> MK66F18
09/25/2020 02:13 PM <DIR> MK80F25615
09/25/2020 02:13 PM <DIR> MKL02Z4
09/25/2020 02:13 PM <DIR> MKL03Z4
09/25/2020 02:13 PM <DIR> MKL13Z644
09/25/2020 02:13 PM <DIR> MKL14Z4
09/25/2020 02:13 PM <DIR> MKL15Z4
09/25/2020 02:13 PM <DIR> MKL16Z4
09/25/2020 02:13 PM <DIR> MKL17Z4
09/25/2020 02:13 PM <DIR> MKL17Z644
09/25/2020 02:13 PM <DIR> MKL24Z4
09/25/2020 02:13 PM <DIR> MKL25Z4
09/25/2020 02:13 PM <DIR> MKL26Z4
09/25/2020 02:13 PM <DIR> MKL27Z4
09/25/2020 02:13 PM <DIR> MKL27Z644
09/25/2020 02:13 PM <DIR> MKL33Z4
09/25/2020 02:13 PM <DIR> MKL33Z644
09/25/2020 02:13 PM <DIR> MKL34Z4
09/25/2020 02:13 PM <DIR> MKL36Z4
09/25/2020 02:13 PM <DIR> MKL43Z4
09/25/2020 02:13 PM <DIR> MKL46Z4
09/25/2020 02:13 PM <DIR> MKM34Z7
09/25/2020 02:13 PM <DIR> MKV10Z1287
09/25/2020 02:13 PM <DIR> MKV10Z7
09/25/2020 02:13 PM <DIR> MKV11Z7
09/25/2020 02:13 PM <DIR> MKV30F12810
09/25/2020 02:13 PM <DIR> MKV31F12810
09/25/2020 02:13 PM <DIR> MKV31F25612
09/25/2020 02:13 PM <DIR> MKV31F51212
09/25/2020 02:13 PM <DIR> MKW01Z4
09/24/2020 03:15 PM <DIR> MKW20Z4
09/25/2020 02:13 PM <DIR> MKW21D5
09/25/2020 02:13 PM <DIR> MKW22D5
09/25/2020 02:13 PM <DIR> MKW24D5
09/24/2020 03:15 PM <DIR> MKW30Z4
09/25/2020 02:13 PM <DIR> MKW40Z4

 

Thanks, 


Roger

0 件の賞賛
返信
1 返信

1,199件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello rogerpease

 

There is no specific driver for the MK10DX64VLH7. One close approach to this one is the MK10D10. You need to be careful with the MCG and clocks configuration, although they are similar the clocks are different.

It is important to add that these drivers are for reference since the MK10DX64xxx7 doesn't have specific SDK.

The MKV10DX64VLH7 belongs to a different family of kinetis and is not recommendable reference for MK10.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信