MED-EKG Tower kit Virtual com Port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MED-EKG Tower kit Virtual com Port

25,121件の閲覧回数
sooryakrishnanu
Contributor III

Hi,

       I bought a twr k53n512 towerkit with med ekg.I use IAR ide for debugging.I am able to flash the code using iar but after flashing when i connect the usb cable to twr-ser board my system shows "USB not recognized".The virtual com port driver provided with medical gui from nxp doesnt work.Is there any solution for my problem?

25 返答(返信)

2,199件の閲覧回数
joicemarkose
Contributor II

Hi Jingjing,

Thanks for the quick reply.

while connecting the twr board without twr ser board, the OSBDM/OSJTAG COM port is visible but unable to download the code.

we were able to download the code by removing   flash loader option through options/Debugger/download/use flash loader. as shown below

still the hello world is not working. :smileysad:

Hope to hear from you soon.

pastedImage_1.pngpastedImage_0.png

0 件の賞賛
返信

2,199件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Joice,

      Sorry for my later reply!

     Please follow this link update your firmware again:

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

     After update the firmware, then uninstall the COM and install it again.

    After you test it , please tell me the result on your side.

Jingjing

0 件の賞賛
返信

2,199件の閲覧回数
sooryakrishnanu
Contributor III

Hi Jingjing,

                    I checked my device with 4 different systems,result was same.I checked in device manger for the usb device it shows no hardware id and shows "code43 error".What does that mean?it has anything to do with my med-ekg tower kit?

0 件の賞賛
返信

2,199件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sooryakrishna U,

    We also need to check the hardware now!

    Could you tell me when you find both the onboard OSJTAG CDC and the TWR-SER USB CDC can't work? in which situation?

   Are you sure, now you still can do K53 programming? And when your just use TWR-K53, without other board, you still can't find the COM port?

  Now, follow this link:

P&E Microcomputer Systems

update your TWR-K53 firmware, and try again.

Wait for your test result!

Jingjing

0 件の賞賛
返信

2,199件の閲覧回数
sooryakrishnanu
Contributor III

Hi Jingjing,

Sorry its not j37 it is j27.

0 件の賞賛
返信