LoRa communication and KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LoRa communication and KL25Z

2,419 次查看
beezee
Contributor III

Hi, 

I want to start a LoRa project with a MCU that I already have (KL25Z). Is there any sample code or project available that I can follow?

I have several LoRa modules like SX1272, RFM95W (868MHz for Europe). But I can be adaptable about which radio I use but I definitely want to set it up by KL46 in kinetis or CodeWarrior. 

Thanks,

Bee Zee

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,065 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Bee Zee,

We don't have example applications using a third party LoRa modules. However, you can start your project by using one of the SPI or UART demo applications included with the KL25Z SDK which can be downloaded from the MCUXpresso SDK Builder.

Additionally, I recommend you to take a look at the newer MCUXpresso IDE as it is replacing KDS.

Best regards,

Gerardo

0 项奖励
回复