LoRa communication and KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LoRa communication and KL25Z

2,372件の閲覧回数
beezee
Contributor III

Hi, 

I want to start a LoRa project with a MCU that I already have (KL25Z). Is there any sample code or project available that I can follow?

I have several LoRa modules like SX1272, RFM95W (868MHz for Europe). But I can be adaptable about which radio I use but I definitely want to set it up by KL46 in kinetis or CodeWarrior. 

Thanks,

Bee Zee

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,018件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Bee Zee,

We don't have example applications using a third party LoRa modules. However, you can start your project by using one of the SPI or UART demo applications included with the KL25Z SDK which can be downloaded from the MCUXpresso SDK Builder.

Additionally, I recommend you to take a look at the newer MCUXpresso IDE as it is replacing KDS.

Best regards,

Gerardo

0 件の賞賛
返信