LIN driver alters GPIO in UART mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN driver alters GPIO in UART mode

2,106件の閲覧回数
ianchuter
Contributor II

Hi 

I have an application running which communicates successfully using the LIN driver on a S9KEAZN16AMLH, however, while the LIN is communicating, the GPIO state is cleared apparently randomly - this stops if the LIN communication stops. The LIN is using UART, so does anyone know why it would be altering the GPIO state?

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,968件の閲覧回数
ianchuter
Contributor II

Hi

Thanks for your reply. This turned out to be an issue with my code - if the interrupt occurred at a certain point the GPIO was being left in a mess - I've restructured this part of my application and it can now ride out the interrupts without issue. 

0 件の賞賛
返信

1,968件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Lan,

   Thanks for your updated information.

   If you still have question about it, just let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,968件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi lan Chuter,

   Do you mean when the LIN UART pin works, the according GPIO input status also changing?

  If yes, the phenomena is correct, because even you configure the pin to other modules function, the GPIO input status also works, it is correct.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信