LCD slowly turn brighter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD slowly turn brighter

1,212 Views
blurblur
Contributor II

Hi,

I am using K30 to drive LCD with charge pump and 8 backplanes. 

My problem is when everytime I change the display, the segment slowly become brighter and will completely turn on after few second.

My question is, which register is controlling the speed of updating the LCD display. Or any other thing that I need to look at. 

Please help. 

Thank you.

0 Kudos
Reply
1 Reply

1,165 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

The LCD frame frequency is controlled by LCD_GCR.LCLK and other clock source selector/divider. But I think your problem maybe not lies on clock speed or frame speed.

K30's LCD module is same as KM34's LCD module. KM34 has TWR board which has a 1/8 duty LCD panel. Please download a KM34 SDK package. There is a SLCD demo in the package. You can refer to the demo and check your software setting and hardware.

If the problem is still there, you can share your code here. I'll help you to solve it.

Regards,

Jing

0 Kudos
Reply