LCD display K60 family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD display K60 family

1,999 Views
wilk
Contributor II

Hi I am using the Kinetis MK60DN256ZVLL10 (k60 Family) and I want to add an external LCD display.

Is it possible to control the LCD using the Freescale eGUI (I want to use the Freescale MQX RTOS btw) ?

Thanks ! :smileyhappy:

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,767 Views
wilk
Contributor II

Problem solved, it's not possible :smileycry:

0 Kudos
Reply

1,767 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

It is possible to connect an smart display as we do with TWR-K60 + TWR-LCD. You can't connect an standard TFT, you would need a K70 for that. But in many cases an smart display connected to Flex bus is a good solution.

Luis

0 Kudos
Reply