Kinetis tool for memory read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis tool for memory read

1,598 Views
vigneshbalaji
Senior Contributor I

Hi,

    Is there any windows tool to read memory of kinetis controller continuously?

0 Kudos
Reply
1 Reply

1,444 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

Thank you for your interest in NXP kinetis product, I would like to provide service for you.
If you want to read the KEA128 memory, you can use the IDE enter the debug mode, then read it in the memory window.
Another way, don't need to use the IDE, you can use the JLINK debugger, then associate with the JLINK Command, after you connect the KEA chip,
input the command: memory address, length
Then the JLINK commander will show the memory data.

Wish it helps you!
If you still have question about it, please kindly let me know!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------