Kinetis k60 watchdog reset occurs even when refreshing correctly.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis k60 watchdog reset occurs even when refreshing correctly.

跳至解决方案
2,649 次查看
kashyapgada
Contributor III

Hello

I am once again facing the Watchdog reset issue with k60 same way as i use to previously. I that time it worked but the same issue has cropped up once again and i dont understand the reason. while i refresh the watchdog and in debugging mode i am able to see it correctly refreshing it still resets. i have pasted my code here. Please someone have a look at it and help me out with the problem.

main.c and wdog.c files pasted

MAIN.c////////////////////////////////////////////

void main(void) {

  disable_irq(45) ;

  Init_Gpio();

gpio_init(PORTB, PTB, 1, OUTPUT); //Buzzer Output

// EnableInterrupts ;

wdog_init();

while(1) {

  delay_wdog(10);

  wdog_refresh();

/*

  Vertical G calculation

*/

  vertical_z_axis_g = z_axis_avg - 1000;

  finalSendData[1] = vertical_z_axis_g/10;

/*

  Lateral G calculation

*/

  lateral_y_axis_g = y_axis_avg;

  finalSendData[2] = lateral_y_axis_g/10;

  }

}

}

///////////////////////////////////////////////////////////////////////////////////////////////////////

WDOG.h

#include "wdog.h"

#include "common.h"    // Common Kinetis defines

void wdog_init(void){

  wdog_unlock();

  WDOG_STCTRLH = WDOG_STCTRLH_DISTESTWDOG_MASK //Disable WDOG Test Mode

  | WDOG_STCTRLH_ALLOWUPDATE_MASK | WDOG_STCTRLH_WDOGEN_MASK | WDOG_STCTRLH_CLKSRC_MASK ; //Allow WDOG CTRL Ref Update

  WDOG_TOVALH = 0x0020;

  WDOG_WINL = WDOG_WINH = 0;

  WDOG_TOVALL = 0x5fff;

// WDOG_PRESC = WDOG_PRESC_PRESCVAL(7);

  WDOG_STCTRLH &= ~(WDOG_STCTRLH_ALLOWUPDATE_MASK) ;

}

void wdog_refresh(void) {

  DisableInterrupts;

  WDOG_REFRESH = WDOG_REFRESH_WDOGREFRESH(WDOG_REFRESH_SEQUENCE_1);

  WDOG_REFRESH = WDOG_REFRESH_WDOGREFRESH(WDOG_REFRESH_SEQUENCE_2);

  EnableInterrupts;

}

void wdog_enable(void){

  delay_wdog(60);

  wdog_unlock();

  delay_wdog(1);

  WDOG_STCTRLH |= WDOG_STCTRLH_WDOGEN_MASK;

  delay_wdog(20);

}

void wdog_unlock(void)

{

  /* NOTE: DO NOT SINGLE STEP THROUGH THIS FUNCTION!!! */

  /* There are timing requirements for the execution of the unlock. If

   * you single step through the code you will cause the CPU to reset.

   */

  /* This sequence must execute within 20 clock cycles, so disable

         * interrupts will keep the code atomic and ensure the timing.

         */

        DisableInterrupts;

  /* Write 0xC520 to the unlock register */

  WDOG_UNLOCK = 0xC520;

  /* Followed by 0xD928 to complete the unlock */

  WDOG_UNLOCK = 0xD928;

  /* Re-enable interrupts now that we are done */

        EnableInterrupts;

}

void wdog_set_timeout(uint32_t time) {

}

void delay_wdog(uint16_t nCount) {

  uint16_t delay = 0;

  for (delay=0;delay<nCount*10;delay++);

}

void wdog_disable(void)

{

  /* First unlock the watchdog so that we can write to registers */

  wdog_unlock();

  /* Clear the WDOGEN bit to disable the watchdog */

  WDOG_STCTRLH &= ~WDOG_STCTRLH_WDOGEN_MASK;

}

标签 (1)
0 项奖励
回复
1 解答
1,619 次查看
kashyapgada
Contributor III

No issues with the WDOG driver code, i found a link within my code where my code did not progress from there at all so the question's answer is bad written code.

also i found this problem by removing (commented) all the code within the while loop and just kept the wdog refresh code and found the it was working properly.

Thanks

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,620 次查看
kashyapgada
Contributor III

No issues with the WDOG driver code, i found a link within my code where my code did not progress from there at all so the question's answer is bad written code.

also i found this problem by removing (commented) all the code within the while loop and just kept the wdog refresh code and found the it was working properly.

Thanks

0 项奖励
回复