Kinetis MKW22D512 minimal boot environment problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis MKW22D512 minimal boot environment problems

1,479 Views
jonathanbartows
Contributor I

Hello. I am trying to program a MKW22D512 on a custom PCB, but I haven't been able to get my JLink JTAG/SWD programmer to recognize the chip on my third PCB. I've wired VDDA, VDD_MCU, VBAT_MCU on the same rail to a 3.3v supply (i.e., pins 38, 32, 25, and 20 are all on a common wire), and the EzPort chip select (pin 36) is pulled high because I'm using a JTAG/SWD programmer. The ground pads and VSSA (pin 28) are both connected to a ground, and the RESET_b pin (pin 41) is connected to ground because it's active low. I've tried connecting and disconnecting the Pierce crystal oscillator circuit (pins 1 and 56) to see if it changed anything, but both times I read a 32 kHz waveform from CLK_OUT. I'm fairly confident that there isn't a fabrication or assembly issue, but when I connect my JLink with the latest software from Segger there are no interfaces found. Is there anything obvious that I'm doing improperly or haven't done to setup the chip for JTAG/SWD programming? Thank you very much for any insight you can offer.

Best,

Jonathan

Labels (1)
0 Kudos
Reply
1 Reply

1,347 Views
DavidS
NXP Employee
NXP Employee

Hi Jonathan,

You state "...and the RESET_b pin (pin 41) is connected to ground ".

If RESET_b connected to ground the debugger will never be able to work.

Yes the reset of the device is active low but you do not want to hold it in that state.  You should have a strong pull-up on RESET_b and the debugger connector can assert the reset signal to get device to known state and enter debugger mode.

I'm not a KW expert but in general all Kinetis devices that I have worked with should be able to connect to debugger and run simple code without any external clock.

Regards,

David

0 Kudos
Reply