Kinetis MK22 Watchdog Refresh Interval

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis MK22 Watchdog Refresh Interval

918件の閲覧回数
LukeJ
Contributor II

This topic has previously been discussed here:
https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV4x-Watchdog-refresh-problem/m-p/776179

For those interested though, I have performed additional testing and would like to share results and welcome feedback for what I may be doing incorrectly.

MCU MK22FN512VLL12
MCU Clock 120MHz
WDOG Source 1KHz LPO
WDOG Windowed mode disabled, using the default settings from SDK 24.12.00 with timeout set to 30 seconds.

My application is super loop based with a typical loop time of 41us.
When WDOG_Refresh is called within the super loop, the timer is never being reset.  I can watch WDOG_TMROUTL count up to 30000 and the watchdog triggers the reset.  So, I began adding delays to the loop.

Adding 800us: The wdog timer is never reset when WDOG_Refresh is called.
Adding 900us: The wdog timer is reset sometimes.  If I log the point of reset, I see WDOG_TMROUTL values between 1ms and 15000ms or so.
Adding 1100us, When I log the point of reset, I see WDOG_TMROUTL values between 1 and 5 or so.

It seems that even 50,000 bus cycles is not sufficient to guarantee the watchdog refresh is successful.

My application is a touchscreen based commercial oven.  It's not going to overheat if the control gets lost for a few minutes and I've not witnessed any lock-ups of the control, so my WDOG refresh period can be relatively long without concern.  This does however seem as though it would be a big problem for other applications.  Therefore, I have to believe this is somehow user error.

By the way, for the past decade or so, minus 2020 through 2022, I've really liked these mcus.

1 返信

879件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @LukeJ ,

Thank you so much for your active participation in our community and for your interest in our products. 

Your detailed sharing is valuable. It's certain that this information will be of great help to many other users who might encounter similar problems. We understand that such exploration often requires a lot of patience and dedication, and we are very grateful for your contribution.

If you have any further findings, ideas, or questions, please don't hesitate to let us know. We're always here to support you and look forward to more interactions with you.

Have a good day,

Celeste

0 件の賞賛
返信