Kinetis L series - DMA channel linking together with activated peripheral DMA request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis L series - DMA channel linking together with activated peripheral DMA request

2,368 次查看
merlin69
Contributor II

Hi!

I'm using Kinetis KL26128Z. Is it possible to use DMA channel linking together with activated peripheral DMA request?

E.g. DMA1 transfer'll start on TPM1 overflow event and also on DMA0 successful transfer (link to DMA1).

Thanks!

Jan

标签 (1)
3 回复数

1,614 次查看
merlin69
Contributor II

The answer is yes.

0 项奖励
回复

1,614 次查看
petermlakar
Contributor I

A sample wold be nice.

I am trying to make a SPI slave with cyclic buffer by  linked DMA channel.

The second DMA hangs after first byte.

    SIM_SCGC6 |= SIM_SCGC6_DMAMUX;//Enable clock gate to the DMA Mux module.

    SIM_SCGC7 |= SIM_SCGC7_DMA;//Enable clock gate to the DMA module

    DMAMUX0_CHCFGn( DMA2) = 0;// reset DMAMUX Read

    DMA_DSR_BCRn( DMA2) = DMA_DSR_BCRn_DONE; // clear/reset DMA status Read

    DMA_DSR_BCRn( DMA3) = DMA_DSR_BCRn_DONE; // clear/reset DMA status Read

    DMAMUX0_CHCFGn( DMA2) = DMAMUX0_CHCFGn_ENBL | // Configure DMAMUX0 Read

                                   DMAMUX0_CHCFGn_SOURCE(DMA_TRIGGER_SPI1_RX);

    DMA_DSR_BCRn( DMA2) = DMA_DSR_BCRn_BCR(0xFFF); // max length of transfer Read

    DMA_SARn( DMA2) = (unsigned int)& SPIx_DL( SPI1);// set source address

    DMA_DARn( DMA2) = (unsigned int)cbuffin; // set destination address

    DMA_DCRn( DMA2) = DMA_DCRn_ERQ |//Enable peripheral request

                             DMA_DCRn_CS | //Cycle steal

                             DMA_DCRn_DINC | //Source increment

                             DMA_DCRn_SSIZE(0x01) |//Source size 8-bit

                             DMA_DCRn_DSIZE(0x01) |//Destination size 8-bit

                             DMA_DCRn_DMOD(0x6) |//Destination address modulo 512bytes

                             DMA_DCRn_LINKCC(0x3) |//link to LCH1 after the BCR decrements to zero

                             DMA_DCRn_LCH1( DMA3) /*|//Link DMA Channel

                             DMA_DCRn_D_REQ*/; //ERQ bit is cleared when the BCR is exhausted

    DMA_DSR_BCRn( DMA3) = DMA_DSR_BCRn_BCR(0xFFF); // max length of transfer Read

    DMA_SARn( DMA3) = (unsigned int)& SPIx_DL( SPI1);// set source address

    DMA_DARn( DMA3) = (unsigned int)cbuffin; // set destination address

    DMA_DCRn( DMA3) = DMA_DCRn_CS | //Cycle steal

                             DMA_DCRn_DINC | //Source increment

                             DMA_DCRn_SSIZE(0x01) |//Source size 8-bit

                             DMA_DCRn_DSIZE(0x01) |//Destination size 8-bit

                             DMA_DCRn_DMOD(0x6) ;//Destination address modulo 512bytes

    SPIx_C2( SPI1) |= SPIx_C2_RXDMAE; //SPI Transmitter DMA enable Write/Read

0 项奖励
回复

1,614 次查看
mjbcswitzerland
Specialist V

Peter

I would like to ask whether you found a solution to your problem?

If I understand it correctly you used one DMA channel to transmit/receive a certain number of bytes and, when its byte count reaches zero, you wanted to start a similar process on a different DMA channel.

I am also looking to do something similar with high speed data where an interrupt after the first buffer is complete is not adequately fast to prepare and start the second task. This means that I also took a look at the linking possibility but my understanding is that it doesn't pass the control to the second DMA channel (which would be the perfect situation and what you look to have needed) but instead the link is more a trigger for the linked DMA channel. This would possiby match with your observations since it would cause a single transfer to take place (noting that there is no trigger otherwise set up in the DMA MUX for your linked channel that would cause a peripheral to trigger it afterwards).

Did you conclude that it wasn't possible or did you find a method for the intended operation?

Regards

Mark

0 项奖励
回复