Kinetis KV10 exposed pad connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KV10 exposed pad connection

2,098 Views
lukasbaumann
Contributor I

Hi,

Can anybody confirm that the exposed pads of Kinetis KV10 devices are isolated from the die?

I can't find any information on the internal connection of the pad in the datasheet.

Thanks,

regards

Lukas

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,925 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Lukas

As normal, the exposed pad will be internal connect to die. So you can connect it to ground. Thanks.

Best Regards

Paul

0 Kudos
Reply

1,925 Views
lukasbaumann
Contributor I

Hi Paul,

Thanks for your reply.

So then the exposed pad should be connected to digital ground? Or might it be better for the analog performance of the chip to connect it to analog ground?

Regards,

Lukas

0 Kudos
Reply

1,925 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Lukas

You can connect to digital ground.

Best Regards

Paul

0 Kudos
Reply