Kinetis K64 Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K64 Ethernet

2,521 Views
punyatagayatri
Contributor II

Hi,

I'm using K64 microcontroller and I need to implement Ethernet , hence I'm using suggested PHY KSZ8081 and RJ45 JX0011D21NL .I want to know how to conenct REF_CLK with microprocessor as pin 72 ( PTA18/EXTAL0/FTM0_FLT2/FTM_CLKIN0 ) is being used by external oscillator to provide clock to microprocessor.

Can someone tell me how to set clock for syncing ethernet PHY and microprocessor?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,077 Views
mjbcswitzerland
Specialist V

Hi

Use the FRDM-K64F circuit diagram as reference.

It connects the EXTAL0 to the PHY's 50MHz REF_CLK.

Make sure that you use the KS8081RNA (generates 50MHz clock form 25MHz crystal) and not the KS8081RND (which requires a 50MHz clock)!!!!

Regards

Mark

0 Kudos
Reply

2,077 Views
punyatagayatri
Contributor II

We are using a cystal to program the microprocessor at this pin so its occupied.Is there any provision to synchronise MAC of processor with PHY Ref Clock.

0 Kudos
Reply

2,077 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

There is an alternative clock source for ENET module, you may feed ENET_1588_CLKIN with 50MHz clock as the same as PHY Ref Clock. Please kindly refer to the following for details.

Untitled.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply