Kinetis K20 safety critical application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K20 safety critical application

2,257 Views
manfredschnell
Contributor IV

Hi,

we think about using a part fo Kinetis K20 subfamily in a safety cirtical application.

Our application has to be compliant with EN 13849 / EN 61508 / EN60730 CLASS B.

We want to reach Class 2 / Performance Level PLr = c @ EN 13849.

Are there any Software packages or White papers available for Kinetis K20 Family?

Best regards

Manfred

Tags (1)
0 Kudos
Reply
2 Replies

2,012 Views
miduo
NXP Employee
NXP Employee

Hi,

Please be note that functional satefy is mainly supported on our auto-product(including KEA serials MCU, M0+ core), please have a check at the following link.

Ultra-Reliable Microcontrollers: Robust, Safe and Secure|NXP 

The Kinetis series (K22, K64, KE) does not support IEC61508. 

2,012 Views
manfredschnell
Contributor IV

Hi Fang Li,

thank you for your answer.

Is there a support plan for IEC61508 ( in my case SIL1 ) with the devices K22, K64?

Best regards

Manfred

0 Kudos
Reply