Kinetis K Datasheet bookmarks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K Datasheet bookmarks

1,930 Views
olli_mannisto
Contributor II

I just downloaded the K65 reference manual, a mighty document with >2000 pages. 

It doesn't come with PDF TOC/bookmarks. 

Personally I'd immediately be put off from using NXP offering if I had a choice of using, say, Texas, NXP and Renesas MCUs a completely random example. Jumping back to the beginning of a huge document to access the TOC is not fun at all.

Plz fix or do something. i.MX 7 series for example has perfectly good PDF TOC.

0 Kudos
Reply
2 Replies

1,849 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Olli Mannisto,

I'm not sure what you mean here.
I can see the Bookmarks of K65 reference manual K65P169M180SF5RMV2.
It is very similar to the reference manual of i.MX 7 series.

Bookmarks.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,849 Views
olli_mannisto
Contributor II

Hmm. Mine doesn't quite look like that. I noticed the K65P169M180SF5RMV2.pdf heading actually contains the TOC. It's not opened automagically and the heading suggests it's not valid so I didn't think of clicking on it. 

So, okay, it's got TOC, it's just a bit oddly formatted. 

K65.png