Kinetis FlexNVM partition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis FlexNVM partition

1,643 Views
LPs
Contributor III

Hi all,

I'm trying to understand how flexNVM partition works.

It seems that th epartition command can not be executed if the memory is already partitioned.

The only way I found is to use Erase All Blocks command before to set a new partition.

Obviously this is not so useful, because of the Erase All Blocks delete my program code also.

What's the correct way to change a partition of a CPU?

Labels (1)
1 Reply

1,238 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

There is no workaround for the mass-erase. The partitioning is supposed to happen only once.

In application note AN4282 - Using the Kinetis Family Enhanced EEPROM functionality chapter 3.1 you will find the next:

Partition.png

Hope this is useful.

Regards!

Jorge Gonzalez

0 Kudos
Reply