Kinetis E microcontroller support in SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis E microcontroller support in SDK

2,053件の閲覧回数
ChrisDarrow
Contributor III


Hello NXP,

Do you intend to add Kinetis E micro support in the SDK going forward?

Thanks,
Chris

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,771件の閲覧回数
DavidS
NXP Employee
NXP Employee

To add to Jorge's statement:

A NXP FAE ported it to KDS and here that is.

Here’s the link to the updated FRDM-KEXX Driver Library Package driver with KDS support for all the example projects

  https://community.freescale.com/docs/DOC-329476

Regards,

David

0 件の賞賛
返信

1,771件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chris Darrow:

Thank you for using our community.

Unfortunately there are currently no plans to add Kinetis E support in KSDK.

For this family NXP has the next software options:

1) Processor Expert drivers: Processor Expert is integrated with Kinetis_Design_Studio. Processor Expert projects generated in KDS can be also used with IAR or Keil:

https://mcuoneclipse.com/2015/06/28/tutorial-using-kinetis-design-studio-v3-0-0-with-iar-and-keil-id...

2) There is a package with baremetal drivers in the next page under "Downloads -> Device Drivers":

Freedom Development Platform for Kinetis KE02|NXP


Best regards,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信