Kinetis Development on a Mac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Development on a Mac

2,107 Views
joetrovato
Contributor I

Hello everyone. I have just inherited a project that uses MQX running on a K70 project. The current developers are with another company using CW on Windows. Is there a way for me to take over this project and continue this development on a Mac? I have looked into using KDS and KSDK but K70 is not supported yet. Similarly, it seems that very few debuggers/programmers have drivers or software for Mac.

Does anyone out there develop MQX projects outside of Windows or CodeWarrior?

Thanks!

0 Kudos
Reply
2 Replies

1,878 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Joe,

Freescale KDS3.0 can support Mac OS 10.10 ("Yosemite").

Kinetis Design Studio Integrated Development |Freescale

other older KDS version and all Codewarrior version don't support MAC OS.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,878 Views
Rick_Li
NXP Employee
NXP Employee

Hi,

CodeWarrior only supported in Windows system, it does not work in MAC OS.

0 Kudos
Reply