Kinetis Controller Not Replying Properly in SPI Slave Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Controller Not Replying Properly in SPI Slave Mode

ソリューションへジャンプ
2,017件の閲覧回数
waqasbutt
Contributor II

Hello,

I am using K20 series controller. In slave mode the controller keeps sending the first value that has been pushed through PUSHR_SLAVE. It never updates.

The slave is receiving data correctly which can be seen through the oscilloscope. The settings CPHA and CPOL also match in slave and master

Images of Oscilloscope

1. Yellow (Clk)

2. Blue    (Slave Out)

3. Purple (Master Out)

4. Green (Chip Select)

DS0001.PNG

DS0002.PNG

Slave Code is as follows

SLAVE:

// Initialization
void SPI1_Init(void)
{
 /* SIM_SCGC6: DSPI1=1 */
 SIM_SCGC6 |= SIM_SCGC6_DSPI1_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x00) |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x0F) |
 SPI_MCR_DIS_TXF_MASK |
 SPI_MCR_DIS_RXF_MASK |
 SPI_MCR_CLR_TXF_MASK |
 SPI_MCR_CLR_RXF_MASK |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_TCR: SPI_TCNT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_TCR = SPI_TCR_SPI_TCNT(0x00);
 /* SPI1_CTAR1: DBR=0,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=0,PASC=0,PDT=0,PBR=0,CSSCK=0,ASC=0,DT=0,BR=0 */
 SPI1_CTAR1 = SPI_CTAR_FMSZ(0x0F) |
 SPI_CTAR_PCSSCK(0x00) |
 SPI_CTAR_PASC(0x00) |
 SPI_CTAR_PDT(0x00) |
 SPI_CTAR_PBR(0x00) |
 SPI_CTAR_CSSCK(0x00) |
 SPI_CTAR_ASC(0x00) |
 SPI_CTAR_DT(0x00) |
 SPI_CTAR_BR(0x00);
 /* SPI1_CTAR0_SLAVE: FMSZ=7,CPOL=0,CPHA=0 */
 SPI1_CTAR0_SLAVE = (uint32_t)((SPI1_CTAR0_SLAVE & (uint32_t)~(uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x18) |
 SPI_CTAR_SLAVE_CPOL_MASK |
 SPI_CTAR_SLAVE_CPHA_MASK
 )) | (uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x07)
 ));
 /* SPI1_SR: TCF=1,TXRXS=1,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=0,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */
 SPI1_SR = SPI_SR_TCF_MASK |
 SPI_SR_TXRXS_MASK |
 SPI_SR_EOQF_MASK |
 SPI_SR_TFUF_MASK |
 SPI_SR_TFFF_MASK |
 SPI_SR_RFOF_MASK |
 SPI_SR_RFDF_MASK |
 SPI_SR_TXCTR(0x00) |
 SPI_SR_TXNXTPTR(0x00) |
 SPI_SR_RXCTR(0x00) |
 SPI_SR_POPNXTPTR(0x00);
 /* SPI1_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_RSER = SPI_RSER_RFDF_RE_MASK;
 /* SPI1_MCR: HALT=0 */
 SPI1_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);
}


// Service Routine
PE_ISR(INT_SPI1_HANDLER)
{
    uint32_t receivedValue = SPI1_POPR;
    uint8_t valueToSend = 0;

   SPI1_SR = SPI_SR_RFDF_MASK | SPI_SR_TCF_MASK;
    if(receivedValue == 0x81)
       valueToSend = 0xF0;
    else
       valueToSend = 0x0F;
   while((SPI1_SR & SPI_SR_TFFF_MASK)==0);
   SPI1_PUSHR_SLAVE = valueToSend;
}
0 件の賞賛
返信
1 解決策
1,828件の閲覧回数
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,829件の閲覧回数
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

0 件の賞賛
返信