KW45 Understanding applications code size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 Understanding applications code size

Jump to solution
2,064 Views
MSM1
Contributor I

Hello,

I would like to know my application code size.

On MCUXpresso the output console shows 174012 which is 170 bytes.

But i dont know if this includes the BLE stack ? kw45b41_nbu_ble_1_9_12_3.sb3 ?

if yes how to know each part size.

Any guide please ? 

Kind Regards,

MSM.

0 Kudos
Reply
1 Solution
2,024 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello MSM,

 

Hope you are doing well.

 

The application code size is the one that the IDE shows.

 

Something important to remark is that the nbu.sb3 is load on the NBU core.

 

I would recommend checking the Getting Started with the KW45B41Z Evaluation Kit | NXP Semiconductors

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
2 Replies
2,024 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello MSM,

 

Hope you are doing well.

 

The application code size is the one that the IDE shows.

 

Something important to remark is that the nbu.sb3 is load on the NBU core.

 

I would recommend checking the Getting Started with the KW45B41Z Evaluation Kit | NXP Semiconductors

 

Regards,

Ricardo

0 Kudos
Reply
2,015 Views
MSM1
Contributor I
Thank you for the reply.
Regards.
MSM.
0 Kudos
Reply