KV5 DMA and UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV5 DMA and UART

1,148 Views
pietrodicastri
Senior Contributor II

Good morning

I imported the example for using the UART and DMA. The original example has the UART0. It works. I changed for using other ports, now I try with UART4 and it does not. I can see the callback called for the and of TX but never for the end of RX. I don t get the point. I am sure the pins and the connections are ok. I am using the tower system for the KV5. 
I drop here the example with minor modifications for changing the UART.

Every help is welcome..

Thank You

Pietro


 

0 Kudos
Reply
2 Replies

1,118 Views
luis_maravilla
NXP Employee
NXP Employee

Hello Pietro

Could you help us confirm which UART-DMA example are you using and which SDK version is it from?

Could you help us share your connections?

Best Regards, Luis

0 Kudos
Reply

1,146 Views
pietrodicastri
Senior Contributor II

The file is here. 

0 Kudos
Reply