KSZ8041 PHY with K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSZ8041 PHY with K60

2,874件の閲覧回数
jonny
Contributor I

I am using the Micrel KSZ8041NL PHY with a K60 tower based custom board.

The PHY schematic matches that of the development boards.

We are finding that with some boards we cant get onto the network when we connect it (via switch or directly to main router). On these boards the link light on the ethernet socket is on as expected but the activity light flashes constantly at around 6Hz (and not with the network activity as I would expect).

Looking at packet capture when connecting by cable via my laptop (shared internet connection) I see dhcp discover packets coming from the board but dhcp offers from the router seem to be ignored.

Is anyone else seeing this same or similar issue or have any ideas as to what might be the cause?

EDIT:

Didnt get to the bottom, nor could micrel after sending our boards to micrel's labs.

For anyones that interested, we got round it by modifying mqx's phy drivers to renegotiate the link speed to 10mbps which was required for the project and found that at 10mbps the problem disappeared.

If anyone else sees this problem let me know as I would like to get the bottom of it either way!

Message was edited by: Jonathan Whyatt

ラベル(1)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

1,332件の閲覧回数
1773750986
Contributor I

I also encountered the same problem, but our application must be 100M. Is there a solution for this 100M application?

0 件の賞賛
返信

1,332件の閲覧回数
1773750986
Contributor I

I also encountered the same problem, but our application must be 100M. Is there a solution for this 100M application?

0 件の賞賛
返信

1,332件の閲覧回数
raffaelerecalca
Contributor I

Hi,

have the same issue doing ifdown;ifup and the workaround is implemented reading if bit 6 of 0x1b register is equal to 1.

If so we hardware reset the ksz8041nl.

In 1110 cycles it appears three times and the workaround fix the problem.

If you have a patch for your renegotiation we try it!

Bye,

Raffaele

0 件の賞賛
返信

1,332件の閲覧回数
jonny
Contributor I

Hi Raffaele,

at least im not the only person to have this problem! That's interesting about the 'Receive Error'.

If you drop me an email, I can send you the patches.

Id also be interested in your project in case there's any similarities in our boards which may  give some clues.

Thanks

J

0 件の賞賛
返信