KL4x SLCD Charge Pump voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL4x SLCD Charge Pump voltage

1,481件の閲覧回数
isaotakashima
Contributor IV

Our customer would like to confirm the voltage of the LCD glass when disable and enable charge pump.

Because their products is battery operated application.

Here is my understanding.

When disable charge pump(CPSEL=0), the voltage of the LCD glass is depends on VDD.

When enable chaege pump(CPSEL=1), the voltage of the LCD glass is depends on LCD_GCR[RVTRIM] value. In other word, they can adjust the voltage of the LCD glass by LCD_GCR[RVTRIM], it voltage is VIREG(0.91V to 1.09V) * 3.

Am I correct?

Please advise as soon as possible.

Best regards,

Takashima

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,342件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Takashima-san

I think you are correct. Thanks.

Best Regards

Paul