[KL26] Power consumption changes after power reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[KL26] Power consumption changes after power reset

1,636 Views
florianackerman
Contributor I

Hi guys,

 

I discovered a weird behaviour on the Kinetis KL26 when switching between power modes. I created a simple test application to illustrate the behaviour. The application simply goes into SLEEP mode (STOP) within an endless mode. It wakes up every 20ms from the low power timer, processes an empty for loop and then goes into sleep again.

 

Now the problem:

When flashing the application to the MCU my oscillator shows an average power consumption of about 3mA. When plugging the power supply off and on again, there's a consumption of about 2mA and the short peaks of the for loop are a lot bigger. This means the processing time of the for loop (1000 iterations) is suddenly very long. Because this doesn't seem weird enough: when changing the MCG mode from PEE to BLPE (all other configuration stay the same), the processing time of the loop is a lot shorter than before. Although the core clock frequency stays the same. Even if the core clock frequency of PEE is a little faster than BLPE, the application seems to need more time for processing the loop.

 

The only hint I may be able to give is the choice of low power mode when in SLEEP. When changing from STOP to PSTOP1 or PSTOP2 the issue with the different PEE power consumptions does not appear, but still PEE has a distinct higher power consumption than BLPE for the same application within the same time slot. The PLL should only need 600µA I guess. But the difference is twice as much.

 

It's very confusing and I hope someone knows if there is a simple explanation behind this!?

 

Kind regards

 

Florian

 

PS: Attached is a test project to illustrate the issue.

Original Attachment has been moved to: Testproject_LowPower.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,491 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I use your attached code tested with FRDM-KL26Z board.

I could measure the 310uA power consumption at FRDM-KL26Z J5 jumper (KL26 power consumption).

It need to stop the software debug and then measure the KL26 power consumption.

test.png

Wish it helps.

BTW: FRDM-KL26Z board related resource could be found here.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply