KL2 programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL2 programming

2,495件の閲覧回数
nishasingh
Contributor I

Whats connections need to be done to program KL2 using universal multilink??

Also what vaule of resistor and capacitor need to put on the Reset pin??

What is the pitch of the programming pins used in the connector for programming kinetisL devices??

Thanks

Nisha

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,278件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Nisha

For resistor and capacitor value of reset pin and debug interface, I think you can reference our freedom board design schematic. Please reference attached.

0 件の賞賛
返信

2,278件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Nishasingh,

KL2 supports SWD interface, and if you use universal multilink, please use the mini 10 port referring to the following snapshot, and size spec is also included.

1.PNG

The recommended resistor and capacitor need to put on the Reset pin can be found in http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KLQRUG.pdf?fpsp=1, you may also refer to the following for details.

2.PNG

Hope that helps,

B.R

Kan

0 件の賞賛
返信