KEA64 Watchdog Inquiry

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA64 Watchdog Inquiry

1,720件の閲覧回数
lim
Contributor II

Hi NXP

The Watchdog is working well when after MCU Reset

but when trying to reconfiguration on main code

we can't enable the watch dog

do you have any idea about that problem? thank you

0 件の賞賛
返信
2 返答(返信)

1,719件の閲覧回数
lim
Contributor II

 

Watchdog Configuration when after MCU reset 

it's working

1234.png

when trying to enable the watchdog on main code

it doesn't working

56.png

  

0 件の賞賛
返信

1,714件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

16.3.2 Configuring the Watchdog.png

You can refer the WDOG example in FRDM-KEAZ Freedom Evaluation Board – QSP(...\FRDM-KEA-QSP\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ128\Driver Test SW for KEAZ128\Driver Test SW for KEAZ128\FRDM_KEA128_WDOG)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信